2.4.2 Using the Library
This topic describes the basic architecture of the Audio 2.0 Function Driver and provides information and examples on its use.
Topics
| Name | Description | 
| Abstraction Model | Describes the Abstraction Model of the USB Audio 2.0 Device Library. | 
| Library Overview | The USB Audio 2.0 Device Library mainly interacts with the system, its clients and function drivers, as shown in the Abstraction Model. The library interface routines are divided into sub-sections, which address one of the blocks or the overall operation of the USB Audio 2.0 Device Library. |