2.5.2 Using the Library
This topic describes the basic architecture of the USB CDC Device Library and provides information and examples on its use.
Topics
| Name | Description | 
| Abstraction Model | Provides an architectural overview of the CDC Function Driver. | 
| Abstract Control Model (ACM) | Describes the various Abstract Control Model (ACM) commands supported by this CDC Function Driver implementation. | 
| Library Overview | The USB CDC Device Library mainly interacts with the system, its clients and function drivers, as shown in the Abstraction Model. The library interface routines are divided into sub-sections, which address one of the blocks or the overall operation of the USB CDC Device Library. | 
| How the Library Works | This section explains the working of the CDC Function Driver Library. |