11.3 Command Complete Event (Opcode – 0x0E)
The BM70/71 module sends the event response to inform the host MCU about the completion of receiving and processing the command. There is a general format for this event that is based on the HCI command the host has issued, and there is a possibility of adding additional parameters to the event response. For more details about the basic format and minimum information returned to the host MCU, see the following tables.