11.5 Number of Completed Packets Event (Opcode – 0x13)
The BM70/71 module sends the event response to the host MCU, informing about the completed data packets for each connection handle since the last time the event was sent to the host. For HCI-ISDAP commands, use this event to indicate the completion of processing the message by the BM70/71 module (format acceptable) but does not indicate finishing of the HCI-ISDAP command operation. The host MCU can use the information in this event response to determine if the device can accept another HCI-ISDAP command. For more details about the format and information returned to the host MCU, see the following tables.