12 Configuration Parameters
This section provides a detailed list and explanation of each programmable parameter in the BM70/71 module. For more details, refer to the BM70/71 Bluetooth Low Energy Module User’s Guide (DS50002542).
There are two distinct modes of operation:
- Auto operation
- Manual operation
The configuration parameters described in this section can affect device behavior in auto operation, manual operation or both. The following sections provide details of the mode of operation affected for each applicable configuration parameter.