5.1 Setting up the Hardware
(Ask a Question)For setting up the hardware, perform the following steps.
- Connect the camera sensor module with the CoaXPress FMC (device) board. This side is called the CXP device side.
- Connect the CoaXPress FMC (host) board with the PolarFire Video Kit through the FMC connector. This side is called the CXP host side.
- Connect the CXP device side and host side.
- Connect the J1 connector of the dual camera sensor module to J1 connector of the CoaXPress FMC (device) board.
- Connect the J11 (FMC) connector of the CoaXPress FMC (host) board to the J14 (FMC) connector of the PolarFire Video Kit.
- Connect the CoaXPress FMC (device) board and the CoaXPress FMC (host) board using the Coaxial HD-BNC to HD-BNC Male to Male cable.
- Connect the HDMI monitor to J1 (HDMI 2.0 transmitter (Tx) port) of the PolarFire Video Kit using the HDMI cable.
- Connect the host PC and the PolarFire Video Kit through J12 of the PolarFire Video Kit using the USB mini cable.
- Connect the FlashPro4 through J21 of CoaXPress FMC (device) board.
- Connect the power supply cable to J20 of the PolarFire Video Kit.
- Ensure that the jumper settings on
the PolarFire Video Kit are same as listed in the following table.
The following table lists the jumper settings of PolarFire Video Kit.
Table 5-1. Jumper and Switch Settings of PolarFire Video Kit Jumper Default Position Description J15 Open SPI Slave and Master mode selection By default, select SPI master
J17 Open 100K PD for TRSTn By default, 1K PD is connected
J19 Pin 1 and 2 Default: XCVR_VREF is connected to GND J28 Pin 1 and 2 Default: Programming through the FTDI J24 Pin 2 and 4 Default: VDDAUX4 voltage is set to 3.3V J25 Pin 3 and 4 Bank4 voltage is set to 2.5V J36 Pin 1 and 2 Default: Board power up through the SW4 SW4 OFF/ON Power ON\OFF slide switch SW6 OFF User slide switch Default position: OFF
J20 12V Input 12V input to the board - Ensure that the following listed
jumper settings are set on the CoaXPress FMC device and host boards.
The following table lists the jumper settings of CoaXPress FMC host and device boards.
Table 5-2. Jumper Settings of CoaXPress FMC Host and Device Board Board Name Jumper Pins CoaXPress FMC host board J20
J19
J14
Closed Pin 2 and 3
Open Pin 2 and 3
Open Pin 2 and 3
CoaXPress FMC device board J7 If Pin 1 and 2 are closed, connect an external power supply of 24V.
If Pin 2 and 3 are closed, the device sources its power from the host through the CoaXPress cable. Ensure that the CoaXPress host is equipped with an external power supply.
- Turn on the HDMI monitor.
- Turn on the board using the SW4 slide switch.
The PolarFire dual camera video and imaging hardware now is set up.