4.4.3.3 Frame Synchronizer
The frame synchronizer block analyzes the demodulated data and compares it to the configured pattern to detect a valid preamble and the start point of a telegram within the data stream.
The frame synchronizer works on a symbol basis. All registers configure and refer to data symbols, not data bits. For hints on bits and symbols, see NRZ and Manchester Coding from Related Links.
The complete hardware is available twice to allow separate configuration and processing of path A and path B. In the following sections, a small x indicates that the description is valid for both paths.
The frame synchronizer is reset at every demodulator restart.
For more details on the description of the required register bits, see Frame Synchronizer Register Description from Related Links.
Pattern Correlation
Two different patterns, each with a length of up to 32 symbols, can be defined to implement a customized Wake Check OK (WCO) and Start of Telegram (SOT) detection procedure.
An example for the correlation process and the pattern match generation for one path is visualized in the following figure.
The demodulated symbol stream is checked in parallel for the configured Wake-up Pattern (WUP) and
Start Frame Identification (SFID). A pattern match is signaled by setting the
corresponding SOTSx.WUPOx or SOTSx.SFIDOx bit to ‘1’. See RX DSP
Control Register Description from Related Links.
The WUP can be configured on a symbol basis in the WUP4x, WUP3x, WUP2x and WUP1x registers. The SFID pattern can be configured on a symbol basis in the SFID4x, SFID3x, SFID2x and SFID1x registers.
The length of each pattern is configurable between 1 and 32 symbols in WUPLx and SFIDLx. If the length of the pattern is configured to be less than 32, the corresponding number of least significant symbols are selected and the rest is ignored.
To create a pattern match, the number of matching symbols has to exceed the threshold values in WUPTx and SFIDCx.SFIDTx. Thus, if the complete pattern is supposed to match, the threshold value has to be one less than the pattern length value.
To avoid an unintended early WUP or SOT, a pattern match will only be indicated if at least the number of symbols configured in the length register was received. Any earlier pattern match is suppressed.
The SIFDCx.SEMEx serial mode enable bit can be used to activate a hardware suppression of an SFID match until a WUP match occurs and a full SFID pattern is received after the WUP.
The data polarity can be configured in DMMx.DMPx. See Demodulator Register Description
from Related Links. If DMPx = 1, the received data are inverted in the
demodulator before they are transferred to the correlator. Therefore, the configured WUP
and SFID pattern must be the inverse of the RF signal.
Configuration example for a WUP and SFID pattern on path A:
DMMA.DMNEA = 0 Data are Manchester-coded
DMMA.DMPA = 1 Manchester polarity: Falling edge in the middle of a bit is ‘1’, data are inverted in the demodulator
WUP4A = 0x80
WUP3A = 0x00
WUP2A = 0x66
WUP1A = 0x66 -> WUP= 1000 0000 0000 0000 0110 0110 0110 0110
WUPLA = 8 -> Only eight LSBs of WUP are considered (0x66) WUPTA = 7 -> Threshold = WUPTA+1 -> All eight symbols must match
SFID4A = 0x00
SFID3A = 0x00
SFID2A = 0x55
SFID1A = 0xA6 -> SFID = 0000 0000 0000 0000 0101 0101 1010 0110
SFIDLA = 16 -> Only 16 LSBs of WUP are considered (0x55A6) SFIDTA = 15 -> Threshold = SFIDTA+1 -> All 16 symbols must match