4.4.3.1 Channel Filter
The correct decimation for each RF band is selected by the CHDN.ADCDN register. The receiving bandwidth is selected by configuring the CHDN.BBDN and CHCR.BWM registers. The following table describes the correct settings for these registers for each bandwidth.
A typical frequency response of the channel filter, including the phase noise effect, is shown in the following figure.
Channel Filter Bandwidths
The register bits CHDN.BBDN and CHCR.BWM are used to select the desired bandwidth. The following table shows the typical bandwidths for an RF signal (fRF) of 433.92 MHz with the corresponding register settings.
|
No. | BW-3 dB, 433.92
-3 dB Bandwidth (fRF =433.92 MHz) |
-30 dB Bandwidth (fRF = 433.92 MHz) |
BBDN |
BWM |
Resulting CLK_BB433.92 Frequency |
|---|---|---|---|---|---|
| 1 | 25 kHz | 41 kHz | 20 | 0 | 75.3 kHz |
| 2 | 27 kHz | 43 kHz | 19 | 0 | 79.3 kHz |
| 3 | 29 kHz | 49 kHz | 17 | 0 | 88.6 kHz |
| 4 | 33 kHz | 55 kHz | 15 | 0 | 100.4 kHz |
| 5 | 35 kHz | 59 kHz | 14 | 0 | 107.6 kHz |
| 6 | 41 kHz | 69 kHz | 12 | 0 | 125.5 kHz |
| 7 | 45 kHz | 75 kHz | 11 | 0 | 136.9 kHz |
| 8 | 50 kHz | 83 kHz | 10 | 0 | 150.6 kHz |
| 9 | 55 kHz | 92 kHz | 9 | 0 | 167.3 kHz |
| 10 | 61 kHz | 103 kHz | 8 | 0 | 188.2 kHz |
| 11 | 71 kHz | 117 kHz | 7 | 0 | 215.1 kHz |
| 12 | 80 kHz | 139 kHz | 7 | 4 | 215.1 kHz |
| 13 | 93 kHz | 151 kHz | 7 | 8 | 215.1 kHz |
| 14 | 99 kHz | 167 kHz | 5 | 1 | 301.2 kHz |
| 15 | 110 kHz | 193 kHz | 5 | 5 | 301.2 kHz |
| 16 | 123 kHz | 205 kHz | 4 | 1 | 376.5 kHz |
| 17 | 134 kHz | 234 kHz | 4 | 5 | 376.5 kHz |
| 18 | 146 kHz | 177 kHz | 5 | 12 | 301.2 kHz |
| 19 | 165 kHz | 270 kHz | 3 | 2 | 502.0 kHz |
| 20 | 185 kHz | 328 kHz | 3 | 6 | 502.0 kHz |
| 21 | 219 kHz | 351 kHz | 3 | 9 | 502.0 kHz |
| 22 | 237 kHz | 368 kHz | 2 | 3 | 753.0 kHz |
| 23 | 243 kHz | 295 kHz | 3 | 13 | 502.0 kHz |
| 24 | 276 kHz | 474 kHz | 2 | 7 | 753.0 kHz |
| 25 | 325 kHz | 494 kHz | 2 | 10 | 753.0 kHz |
| 26 | 366 kHz | 446 kHz | 2 | 14 | 753.0 kHz |
Bandwidth Scaling
The channel filter is realized as a digital filter and the sampling rate depends on the RF signal. It is, therefore, subject to scaling with the RF signal and the corresponding sampling clock (CLK_BB). This scaling effect can modify the actual -3 dB and -30 dB bandwidth in the range of -5.6% to +3.6% versus the typical bandwidths given for fRF = 433.92 MHz in the preceding table.
- The target division factor
(DIV_IF) is selected from the following table.
Table 4-9. Frequency Dependent Division Factor (DIV_IF) No. fRF DIV_IF 1 310 MHz to 318 MHz 204 2 418 MHz to 440 MHz 288 3 441 MHz to 477 MHz 306 4 836 MHz to 870 MHz 576 5 871 MHz to 956 MHz 612 - The target (-3 dB) bandwidth is selected, and the corresponding BBDN and CLK_BB433.92 are remembered. See Filter Settings for Each Supported Bandwidth in the Channel Filter from Related Links.
- The application sampling clock,
CLK_BBAPPL, for the target application frequency,
fRF,APPL, calculate by using the following formula:
- Calculate the resulting
frequency-dependent scaling factor by using the following
formula:
- Apply the scaling to the typical
bandwidth
- If the resulting BWAPPL is too narrow for the target data rate, deviation and crystal tolerances, restart the procedure must at the next higher bandwidth.
The application has a target application frequency of fRF = 316 MHz and requires a bandwidth of 366 kHz.
- DIV_IF = 205 is taken from line 1 of the preceding table
- BBDN = 2 and CLK_BB433.92 = 753.0 kHz are taken from line 26, see Filter Settings for Each Supported Bandwidth in the Channel Filter from Related Links.
- The application sampling clock is calculated using
- The resulting scaling is calculated using
- Apply the scaling to the typical bandwidth