6.24.9 iswctype Function
Test the property of a wide character.
Include
<wctype.h>
Prototype
int iswctype(wint_t wc, wctype_t desc);
Arguments
-
wc - The wide character to test.
-
desc - The wide character property to test for.
Return Value
Returns a non-zero integer value if the wide character, wc, has the property
described by desc; otherwise, returns a zero.
Remarks
See wctype Function, which can be used to obtain a description of the desired wide character property.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <wctype.h>
#include <stdio.h>
#include <stdbool.h>
int main(void)
{
wchar_t wStr[] = L"A string, 2 wide 4 some.\n";
wint_t wc;
unsigned idx = 0;
bool found = false;
do {
wc = wStr[idx];
if(iswctype(wc, wctype("space"))) {
if( ! found)
printf("Found matching wide char at position: ");
printf("%s%u", found ? ", " : "", idx);
found = true;
}
idx++;
} while(wStr[idx]);
printf("\n");
}
Example Output
Found matching wide char at position: 1, 9, 11, 16, 18, 24