6.24.21 wctrans Function
Returns a value that describes a mapping between wide characters and that can be used by
towctrans().
Include
<wctype.h>
Prototype
wctrans_t wctrans(const char * property);
Argument
-
property - The wide character mapping property.
Return Value
Returns a value with type wctrans_t that describes a mapping of wide
characters identified by the string argument, property
Remarks
The string arguments are shown in the following table along with the wide character function which maps with the same wide character property.
String argument to wctrans() | Function that maps with the same wide character property |
|---|---|
"tolower" | towlower() |
"toupper" | towupper() |
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <wctype.h>
#include <wchar.h>
#include <stdio.h>
int main(void)
{
wchar_t wStr[] = L"A string, 2 wide 4 some.\n";
wint_t wc;
unsigned idx = 0;
printf("String in upper case: ");
do {
wc = wStr[idx];
putwchar(towctrans(wc, wctrans("toupper")));
idx++;
} while(wStr[idx]);
printf("\n");
}Example Output
String in upper case: A STRING, 2 WIDE 4 SOME.