6.19.7 abs Function
Calculates the absolute value.
Include
<stdlib.h>
Prototype
int abs(int i);
Argument
i- integer value
Return Value
Returns the absolute value of i.
Remarks
A negative number is returned as positive; a positive number is unchanged.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdio.h>
#include <stdlib.h>
int main(void)
{
int i;
i = 12;
printf("The absolute value of %d is %d\n", i, abs(i));
i = -2;
printf("The absolute value of %d is %d\n", i, abs(i));
i = 0;
printf("The absolute value of %d is %d\n", i, abs(i));
}
Example Output
The absolute value of 12 is 12
The absolute value of -2 is 2
The absolute value of 0 is 0