6.19.18 getenv Function
Get a value for an environment variable.
Attention: This function is not
implemented by MPLAB XC8 C compilers.
Include
<stdlib.h>
Prototype
char * getenv(const char * name);
Argument
name- name of environment variable to read
Return Value
Returns a pointer to the value of the environment variable if successful; otherwise, returns a null pointer.
Remarks
This function must be customized to be used as described (see
pic30-libs). By default, there are no entries in the environment list
for getenv to find.
Example
#include <stdio.h>
#include <stdlib.h>
int main(void)
{
char *incvar;
incvar = getenv("INCLUDE");
if (incvar != NULL)
printf("INCLUDE environment variable = %s\n", incvar);
else
printf("Cannot find environment variable INCLUDE ");
}
Example Output
Cannot find environment variable INCLUDE