6.19.1 stdlib.h Types and Macros
div_t
A type that holds a quotient and remainder of a signed integer division
with operands of type int.
Prototype
typedef struct { int quot, rem; } div_t;
Remarks
This is the structure type returned by the function, div().
ldiv_t
A type that holds a quotient and remainder of a signed integer division
with operands of type long.
Prototype
typedef struct { long quot, rem; } ldiv_t;
Remarks
This is the structure type returned by the function, ldiv().
lldiv_t
A type that holds a quotient and remainder of a signed integer division with operands
of type long.
Prototype
typedef struct { long long quot, rem; } lldiv_t;
Remarks
This is the structure type returned by the function, lldiv().
EXIT_FAILURE
Reports unsuccessful termination.
Remarks
EXIT_FAILURE is a value for the exit function to return
an unsuccessful termination status.
Example
See exit for example of use.
EXIT_SUCCESS
Reports successful termination.
Remarks
EXIT_SUCCESS is a value for the exit function to return
a successful termination status.
Example
See exit() for example of use.
MB_CUR_MAX
Maximum number of characters in a multibyte character.
Value
1
RAND_MAX
Maximum value capable of being returned by the rand() function.
Value
32767