6.19.17 free Function
Frees dynamically allocated memory.
Include
<stdlib.h>
Prototype
void free(void * ptr);
Argument
ptr- pointer to the memory to be freed
Remarks
Frees memory previously allocated with calloc, malloc or
realloc. If free is used on space that has already been
deallocated (by a previous call to free or by realloc) or on
space not allocated with calloc, malloc or
realloc, the behavior is undefined.
When using the simple implementation of dynamic memory allocation, only a rudimentary merging of freed memory blocks is performed. See your MPLAB XC compiler User's Guide for more information on how dynamic memory allocation is implemented with your compiler.
Example
#include <stdio.h>
#include <stdlib.h>
int main(void)
{
long *i;
if ((i = (long *)malloc(50 * sizeof(long))) == NULL)
printf("Cannot allocate memory\n");
else
{
printf("Memory allocated\n");
free(i);
printf("Memory freed\n");
}
}
Example Output
Memory allocated
Memory freed