6.19.13 bsearch Function
Performs a binary search.
Include
<stdlib.h>
Prototype
void *bsearch(const void *key, const void
*base, size_t nelem, size_t size, int
(*cmp)(const void *ck, const void
*ce));
Arguments
key- object to search for
base- pointer to the start of the search data
nelem- number of elements
size- size of elements
cmp- pointer to the comparison function
Arguments to the comparison function are as follows.
ck- pointer to the key for the search
ce- pointer to the element being compared with the key
Return Value
Returns a pointer to the object being searched for if
found; otherwise, returns NULL.
Remarks
The value returned by the compare function is <0 if
ck is less than ce, 0 if
ck is equal to ce or >0 if
ck is greater than ce.
In the following example, qsort is used
to sort the list before bsearch is called.
bsearch requires the list to be sorted
according to the comparison function. This comp
uses ascending order.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdlib.h>
#include <stdio.h>
#define NUM 7
int comp(const void *e1, const void *e2);
int main(void)
{
int list[NUM] = {35, 47, 63, 25, 93, 16, 52};
int x, y;
int *r;
qsort(list, NUM, sizeof(int), comp);
printf("Sorted List: ");
for (x = 0; x < NUM; x++)
printf("%d ", list[x]);
y = 25;
r = bsearch(&y, list, NUM, sizeof(int), comp);
if (r)
printf("\nThe value %d was found\n", y);
else
printf("\nThe value %d was not found\n", y);
y = 75;
r = bsearch(&y, list, NUM, sizeof(int), comp);
if (r)
printf("\nThe value %d was found\n", y);
else
printf("\nThe value %d was not found\n", y);
}
int comp(const void *e1, const void *e2)
{
const int * a1 = e1;
const int * a2 = e2;
if (*a1 < *a2)
return -1;
else if (*a1 == *a2)
return 0;
else
return 1;
}
Example Output
Sorted List: 16 25 35 47 52 63 93
The value 25 was found
The value 75 was not found