6.19.35 strtoll Function
Convert string to long long integer value.
Include
<stdlib.h>
Prototype
long long int strtoll( const char * restrict nptr, char ** restrict
endptr, int base);
Arguments
nptr- the string to attempt to convert
endptr- pointer to the remainder of the string that was not converted
base- The base of the conversion
Return Value
The converted value, or 0 if the conversion could not be performed.
Remarks
The strtoll function attempts to convert the first part
of the string pointed to by nptr to a long long
integer value.
Any initial whitespace characters in the string are
skipped. The following characters representing the integer are assumed to be in a
radix specified by the base argument. Conversion stops once an
unrecognized character is encountered in the string. If the correct converted value
is out of range, the value of the macro ERANGE is stored in
errno.
If the value of base is zero, the characters
representing the integer can be in any valid C constant form (i.e., in decimal,
octal, or hexadecimal), but any integer suffix is ignored. If the value of base is
between 2 and 36 (inclusive), the expected form of the integer characters is a
sequence of letters and digits representing an integer with the radix specified by
base, optionally preceded by a plus or minus sign, but again,
the integer suffix is ignored. The letters from a (or
A) through z (or Z) are
ascribed the values 10 through 35; only letters and digits whose ascribed values are
less than that of base are permitted. If the value of
base is 16, the characters 0x or
0X may optionally precede the sequence of letters and digits,
following the sign if present.
When using MPLAB XC8, the function will set errno to
EINVAL and return 0 if base is invalid.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdlib.h>
#include <stdio.h>
int main(void)
{
char * string = "-1234abcd";
char * final;
long long result;
result = strtoll(string, &final, 10);
printf("The integer conversion of the string \"%s\" is %lld; final string part is \"%s\"\n", string, result, final);
}
Example Output
The integer conversion of the string "-1234abcd" is -1234; final string part is "abcd"