3.7 Media Redundancy Protocol Configuration
Use this command to create and configure a Media Redundancy Protocol (MRP) instance.
Command Syntax:
Ring configuration commands:
media-redundancy <inst>
role { mrc | mrm | mra }
mrm priority <prio>
mrm react-on-link-change
name <name>
uuid <uuid>
oui { default | siemens | custom <custom_oui> }
recovery-profile { 10ms | 30ms | 200ms | 500ms }
port1 interface <port_type> <port>
port2 interface <port_type> <port>
admin-state { enable | disable }Argument | Description | |
Parameter |
| ERPS instance number in the range of 1–6. |
| Set this node to be a Media Redundancy Client (MRC), Media Redundancy Manager (MRM), or Media Redundancy Auto Manager (MRA) | |
| If role is 'mrm', valid values are 0x0000, 0x1000–0x7000, 0x8000. If role is 'mra', valid values are 0x9000–0xF000, 0xFFFF. Smaller values give higher priority. | |
| Domain name for this media-redundancy instance (1–240 characters enclosed in double-quotes) | |
| Universally Unique Identifier (UUID) in the form XXXXXXXX-XXXX-XXXX-XXXX-XXXXXXXXXXXX, where each ‘X’ represents a hexadecimal digit, and it must be enclosed in double quotes. | |
| OUI to use in MRP_Option TLVs | |
| Port type and ID assigned to ring port1 and/or ring port2 | |
Default | None | |
Mode | Media-redundancy mode | |
Usage | Configure MRP parameters. To delete the specific MRP instance, use the ‘no’ version of the command, or use parameter ‘all’ to delete all MRP instances. | |
Example | Example 1: Create MRP instance 1 with a manager role, specify port1 and port2 interfaces and enable MRP instance. | |
Signal Fail Trigger for ring port1/port2 and Interconnection configuration commands:
port1 sf-trigger { link | { mep domain <md_name> service <ma_name> mep-id <mepid> } }
port2 sf-trigger { link | { mep domain <md_name> service <ma_name> mep-id <mepid> } }
interconnection role { mic | mim | none }
interconnection sf-trigger { link | { mep domain <md_name> service <ma_name> mep-id <mepid> } }Argument | Description | |
Parameter |
| The MEP’s domain name <kword1–15> |
| The MEP's service name within the domain <kword1–15> | |
| The MEP's MEP-ID in the range of 1–8191. | |
| Media Interconnection Client (MIC), Media Redundancy Interconnection Manager (MIM) or none. | |
Default | port1/port2's signal fail trigger default (link). Disable interconnection functionality on this node | |
Mode | Media-redundancy mode | |
Usage | Configure MRP Signal Fail Trigger and Interconnection. To set default, use the 'no' version of the command. | |
Example | Example 1: Create MRP instance 1 and set signal fail trigger on port1 to link. | |