3.16 MVR Configuration
Use this command to configure Multicast VLAN Registration (MVR) protocol.
Command Syntax:
mvr
mvr name <vlan_name> channel <channel_profile>
mvr name <vlan_name> { election | igmp-address <ipv4_ucast> }
mvr name <vlan_name> mode { dynamic | compatible }
mvr name <vlan_name> frame tagged
mvr name <vlan_name> frame priority <priority>
mvr name <vlan_name> last-member-query-interval <lmqi>
mvr { vlan <vlan_list> | name <vlan_name> } type { source | receiver }
mvr vlan <vlan_list> channel <channel_profile>
mvr vlan <vlan_list> [ name <vlan_name> ]
mvr vlan <vlan_list> { election | igmp-address <ipv4_ucast> }
mvr vlan <vlan_list> mode { dynamic | compatible }
mvr vlan <vlan_list> frame tagged
mvr vlan <vlan_list> frame priority <priority>
mvr vlan <vlan_list> last-member-query-interval <lmqi>
mvr immediate-leaveArgument | Description | |
Parameter |
| MVR multicast VLAN name |
| Profile name in 16 characters | |
| A valid IPv4 unicast address | |
| CoS priority ranges from 0 to 7 | |
| The range is from 0 to 31744. The default Last Member Query Interval (LMQI) is 5 tenths or one-half second. | |
Default | N.A | |
Mode | Global Configuration mode and Port List Interface mode (for type and immediate leave settings) | |
Usage | Enable/disable MVR and interface settings | |
Example | Example 1: Enable MVR and add testmvr profile. Example 2: Set port 2 type as source and enable immediate leave setting. | |