3.3 Ports Configuration Commands
Configure Port Speed, Advertise Duplex, Advertise Speed, Flow Control, PFC (Priority Flow Control), Maximum Frame Size, Excessive Collision mode, and Frame Length Check.
Use this command to enable/disable Ethernet port (has no effect on PoE power).
Command Syntax:
shutdownArgument | Description | |
Parameter | N.A | N.A |
Default | N.A | |
Mode | Port List Interface Configuration mode | |
Usage | Use the command to disable the specified interface and use ‘no’ form of this command to enable the interface. | |
Example | Example 1: Disable port 1. Example 2: Disable ports 1 through 4. Example 3: Enable all ports. | |
Use this command to configure the port speed.
Command Syntax:
speed { 10 | 100 | 1000 | auto { [ 10 ] [ 100 ] [ 1000 ] { [ no-hdx ] | [ no-fdx ] } } }Argument | Description | |
Parameter |
| 10 Mbps |
| 100 Mbps | |
| 1000 Mbps (1 Gbps) | |
| Auto negotiation | |
| Only advertise full duplex | |
| Only advertise half duplex | |
Default | All ports are set to Auto | |
Mode | Port List Interface mode | |
Usage | Use this command to set the speed of the specified interface. | |
Example | Example 1: Set speed for port 1 to 100 Mbps. Example 2: Set all ports to 1 Gbps. | |
Use this command to configure the interface duplex mode.
Command Syntax:
duplex { half | full | { auto [ half | full ] } }Argument | Description | |
Parameter |
| Half duplex when speed is forced (non-auto) |
| Full duplex when speed is forced (non-auto) | |
| Auto negotiation of duplex mode (obsolete, but still supported in startup-config) | |
Default | All ports are set to Auto | |
Mode | Port List Interface mode | |
Usage | Use to set the duplex mode of the specified interface. To set duplex to the default, use the ‘no’ form of the command. | |
Example | Example 1: Set duplex for port 1 to half. | |
This command configures the flow control for the interface (to slow packet transition temporarily upon request, or, for packet reception, to signal the remote transmitter to temporarily slow down its packet transition whenever switch reception buffer becomes to full). PFC and flowcontrol cannot both be enabled on the same port.
Command Syntax:
flowcontrol { on | off }
priority-flowcontrol prio <prio>Argument | Description | |
Parameter |
| Enable flowcontrol. |
| Disable flowcontrol. | |
| Range of priorities (for example, 0–4,7) | |
Default | All ports flow control receive and send is off. Priority flowcontrol is off | |
Mode | Port List Interface mode | |
Usage | Use to set the flow control and PFC for the interface. To revert to the default, use the ‘no’ form of the command. | |
Example | Example 1: Enable flowcontrol for port 1. Example 2: Enable priority flowcontrol with 0–3 priorities for all ports. | |
Use this command to specify maximum Ethernet frame size for the interface.
Command Syntax:
mtu <max_length>Argument | Description | |
Parameter |
| Maximum frame size in bytes. The range is 1518–10240 bytes. |
Default | All ports mtu 10240 bytes | |
Mode | Port List Interface mode | |
Usage | Use to set the maximum frame size for the interface. To return to the default, use the ‘no’ form of the command. | |
Example | Example 1: Set mtu for port 1 to 1518. Example 2: Set mtu for all ports to 1518. | |
Use this command to configure port transmit collision behavior.
Command Syntax:
excessive-restart Argument | Description | |
Parameter | N.A | N.A |
Default | Discard frame after 16 collisions | |
Mode | Port List Interface mode | |
Usage | Use to set the maximum frame size for the interface. To return to the default, use the ‘no’ form of the command. | |
Example | Example 1: Restart backoff algorithm after 16 collisions for port 1. Example 2: Discard frame after 16 collisions for all ports. | |
This command configures if frames with incorrect frame length in the EtherType/Length field shall be dropped.
Command Syntax:
frame-length-checkArgument | Description | |
Parameter | N.A | N.A |
Default | None | |
Mode | Port List Interface mode | |
Usage | Drop frames with mismatch between EtherType/Length field and actual payload size. To disable the frame check, use the ‘no’ form of the command. | |
Example | Example 1: Disable frame length check for port 1. Example 2: Enable frame length check for all ports. | |