6.4 Project Selection Page
This page shows the list of various project types that can be chosen.

-
Generic Project
Continuing the wizard after choosing this option creates a custom project that has system/device initialization code and various software modules added to the project. The application logic can be easily added that could use the generated code.
-
Low Power Periodic Transmission of Data
This project demonstrates the periodic wireless transmissions and low power sleep modes. In this application, the system will be in a sleep mode (that consumes very little power), wake up after a pre-determined time to transmit a data (i.e., power supply voltage value read from the transceiver), and go back into sleep mode.
-
Performance Analyzer
This project creates the Performance Analyzer firmware for the target boards, using which, the performance tests such as PER, ED Scan, Range Test etc. can be performed.
-
Wireless UART
This project demonstrates the implementation of a bidirectional Wireless UART that enables debugging and communication between two systems wirelessly.