6.9 Select Modules Page
This page lists a set of firmware code modules that can be optionally added to the project. This creates a framework that can be enhanced further by adding application logic. The following are the supported firmware modules:
| Category | Name of the module |
|---|---|
| Debugging | USART serial communication |
| Periodic Operations | Periodic Operations Using Timer |
| Low Power Sleep And Wake mechanism | |
| Transceiver Feature Access | Transceiver Features |
| User Interface | LED |
| Push Button |
Click on the button Next to view Summary Page.