6.11 Wireless Project
In the Project Wizard, click on the button Finish to generate a project. A solution is created with a project under it. The project contains all the required files. After making the desired modifications to the code (add application logic to 'usr_' files), build the project and flash the binary file to the device.
The following sections shows the project structure and describes how to start making modifications.