2.3.2 VectorConvolve

Description

VectorConvolve computes the convolution between two source vectors and stores the result in a destination vector. The result is computed as follows:

Where,

x[k] = source one vector of size N,

h[k] = source two vector of size M (with M < N).

Prototype

fractional* VectorConvolve (int numElems1,int numElems2,fractional* dstV, fractional* srcV1,fractional* srcV2);

Arguments

Parameters

Description

numElems1

Number of elements in source one vector

numElems2

Number of elements in source two vector

dstV

Pointer to the destination vector

srcV1

Pointer to the source one vector

srcV2

Pointer to the source two vector

Returns

Pointer to the base address of the destination vector.

Remarks

The number of elements in the source two vector must be less than or equal to the number of elements in the source one vector.

The destination vector must already exist, with exactly numElems1+numElems2-1 number of elements.

This function can be self-applicable.

Source File

  • vcon_aa.s

Function Profile

Device

Program Words

Cycles

PIC32A

37

For N = numElems1, and M = numElems2,

System resource usage

  • W0… W7 - used, not restored
  • W8…W9 - saved, used, restored
  • ACCA - used, not restored
  • CORCON - saved, used, restored
  • Two REPEAT instruction(s)