2.3.1 VectorAdd
Description
VectorAdd adds the value of each element in the source one vector with its counterpart in the source two vector and places the result in the destination vector.
Prototype
fractional* VectorAdd (int numElems, fractional* dstV, fractional* srcV1, fractional* srcV2);
Arguments
|
Parameters |
Description |
|---|---|
|
numElems |
Number of elements in the source vectors |
|
dstV |
Pointer to the destination vector |
|
srcV1 |
Pointer to the source one vector |
|
srcV2 |
Pointer to the source two vector |
Returns
Pointer to the base address of the destination vector.
Remarks
If the absolute value of srcV1[n] + srcV2[n] is larger than the maximum value of 1.31 fractional datatype, this operation results in saturation for the nth element.
This function can be computed in place.
This function can be self-applicable.
Source File
- vadd_aa.s
Function Profile
|
Device |
Program Words |
Cycles |
|---|---|---|
|
PIC32A |
11 |
36 + 4*(numElems) |
System resource usage
- W0…W4 - used, not restored
- ACCA - used, not restored
- CORCON - saved, used, restored
- REPEAT instruction(s) usage – None