2.3.13 VectorZeroPad
Description
VectorZeroPad copies the contents of the source vector into the beginning of the destination vector, and then fills the remaining positions—specified by numZeros — with zeros to complete the destination vector.
dstV[n] = srcV[n], 0 ≤ n < numElems
dstV[n] = 0, numElems ≤ n < numElems + numZeros
Prototype
fractional* VectorZeroPad (int numElems, int numZeros, fractional* dstV, fractional* srcV1);
Arguments
|
Parameters |
Description |
|---|---|
|
numElems |
Number of elements in the source vectors |
|
numZeros |
Number of zeros |
|
dstV |
Pointer to the destination vector (of size numElems + numZeros) |
|
srcV1 |
Pointer to the source vector |
Returns
Pointer to the base address of the destination vector.
Remarks
The destination vector must already exist with exactly numElems + numZeros number of elements.
This function can be computed in place.
This function uses VectorCopy.
Source File
- vzpad_aa.s
Function Profile
|
Device |
Program Words |
Cycles |
|---|---|---|
|
PIC32A |
9 |
12 + (numZeros) |
- The above-mentioned program word and cycle counts pertain solely to VectorZeroPad. However, as this function inherently utilizes VectorCopy, the respective counts for VectorCopy must also be considered.
- In the description of VectorCopy, the number of cycles reported includes four cycles of C-function call overhead. Thus, the number of actual cycles from VectorCopy to add to VectorZeroPad is four less than whatever number is reported for a stand-alone VectorCopy.
System resource usage
- W0…W5 - used, not restored
- One REPEAT instruction(s)