1.5.5.4.20 SRV_FU_CfgWrite Function
C
void SRV_FU_CfgWrite(void *src, uint16_t size);
Summary
Writes the firmware upgrade information.
Description
This function is used to write the firmware upgrade information, which is stored out of the PRIME stack.
Precondition
The SRV_FU_Initialize function should have been called before calling this function..
Parameters
| Param | Description |
|---|---|
|
src |
Pointer to the buffer with the information to write |
|
size |
Number of bytes to write |
Returns
None.
Example
uint32_t fuData[3];
SRV_FU_CfgWrite(&fuData, sizeof(fuData));
Remarks
This function is called by the PRIME stack.