1.5.5.4.26 SRV_FU_RegisterCallbackVerify Function
C
void SRV_FU_RegisterCallbackVerify(SRV_FU_IMAGE_VERIFY_CB callback);
Summary
Registers a function to be called back when the received image has been verified.
Description
This routine allows the PRIME stack to register a function to be called back when the received image has been verified.
Precondition
The SRV_FU_Initialize function should have been called before calling this function..
Parameters
| Param | Description |
|---|---|
|
callback |
Pointer to the callback function |
Returns
None.
Example
void _image_verification(SRV_FU_VERIFY_RESULT verifyResult)
{
...
}
void main(void)
{
SRV_FU_Initialize();
SRV_FU_RegisterCallbackVerify(_image_verification);
}
Remarks
This function is called by the PRIME stack.