1.5.5.4.16 SRV_FU_End Function
C
void SRV_FU_End(SRV_FU_RESULT fuResult);
Summary
Ends the firmware upgrade process.
Description
This function is used to finish the firmware upgrade process and to trigger the execution of the new firmware.
Precondition
The SRV_FU_Initialize function should have been called before calling this function..
Parameters
| Param | Description |
|---|---|
|
fuResult |
Result of the firmware upgrade process |
Returns
None.
Example
SRV_FU_End(SRV_FU_RESULT_SUCCESS);
Remarks
This function is called by the PRIME stack.