2.3 Clocking Structure
(Ask a Question)The following figure shows the clocking structure of the demo design.
As shown in the preceding figure, the on-board 50 MHz crystal oscillator
provides a reference clock to the PF_CCC_C0 block. PF_CCC_C0 generates the following
clocks:
- 200 MHz clock that drives all the blocks of top_0 and PFSOC_DSP_FLOW_TOP
- 25 MHz slow clock is a secondary clock needed by the CoreFFT block which is within the PFSOC_DSP_FLOW_TOP