Configure the Access Management table on the Access Management Configuration page, as shown in the following figure. The maximum number of entries is 16. If the application's type matches any one of the access management entries, then it allows access to the switch.Figure 4-38. Access Management Configuration
The Access Management Configuration page has the following parameters:
Mode: Indicates the access management mode operation. Possible modes are:
Delete: Check to delete the entry. It is deleted during the next save.
VLAN ID: Indicates the VLAN ID for the access management entry
Start IP Address: Indicates the start IP unicast address for the access management entry
End IP Address: Indicates the end IP unicast address for the access management entry
HTTP/HTTPS: Indicates that the host can access the switch from HTTP/HTTPS interface, if the host IP address matches the IP address range provided in the entry
SNMP: Indicates that the host can access the switch from SNMP interface, if the host IP address matches the IP address range provided in the entry
Telnet/SSH: Indicates that the host can access the switch from TELNET/SSH interface, if the host IP address matches the IP address range provided in the entry