5.1.4 Monitor System IP Status
The Monitor > System > IP Status page displays the status of the IP protocol layer. The status is defined by the IP interfaces, the IP Routes (IPv4 and IPV6), and the neighbor cache (ARP cache) status. See the following figure.

The list of parameters is as follows:
- IP Interfaces
- Interface: The name of the interface
- Type: The address type of the entry. This may be LINK, IPv4, or IPv6.
- Address: The current address of the interface (of the given type)
- Status: The status flags of the interface (and/or address)
- IP Routes
- Network: The destination IPv4/IPv6 network or host address of this route
- Gateway: The gateway address of this route
- Status: The status flags of the route
- Neighbor Cache
- IP Address: The IPv4/IPv6 address of the entry
- Link Address: The Link (MAC) address for which a binding to the IP address given exists