4.11.1 Aggregation Common Configuration
The Common Aggregation Configuration page is used to configure the Aggregation hash mode. This mode applies to the whole network element.
The Common Aggregation Configuration page has the following parameters:
- Source MAC Address: Used to calculate the destination port for the frame. Check to enable the use of the Source MAC address or uncheck to disable. By default, Source MAC Address is enabled.
- Destination MAC Address: Used to calculate the destination port for the frame. Check to enable the use of the Destination MAC Address or uncheck to disable. By default, Destination MAC Address is disabled.
- IP Address: Used to calculate the destination port for the frame. Check to enable the use of the IP Address or uncheck to disable. By default, IP Address is enabled.
- TCP/UDP Port Number: Used to calculate the destination port for the frame. Check to enable the use of the TCP/UDP Port Number or uncheck to disable. By default, TCP/UDP Port Number is enabled.