4.10.2.6.3 Network ARP Inspection Static Table Configuration
The Static ARP Inspection Table page shows the static ARP Inspection rules. The maximum number of rules is 256 on the switch.
The Static ARP Inspection Table page has the following parameters:
- Delete: Check to delete the entry. It is deleted during the next save.
- Port: The logical port for the settings
- VLAN ID: The VLAN ID for the settings
- MAC Address: Allowed Source MAC address in ARP request packets
- IP Address: Allowed Source IP address in ARP request packets