EAPOL Counters:Figure 5-38. EAPOL CountersThese supplicant frame counters are available for the following administrative states:
Force Authorized
Force Unauthorized
Port-based 802.1X
Single 802.1X
Multi 802.1X
Backend Server Counters:Figure 5-39. Backend Server CountersThis backend (RADIUS) frame counters are available for the following administrative states:
Port-based 802.1X
Single 802.1X
Multi 802.1X
MAC-based Auth.
Last Supplicant/Client Information:Figure 5-40. Last Supplicant/Client InformationInformation about the last supplicant/client that attempted to authenticate. This information is available for the following administrative states:
Port-based 802.1X
Single 802.1X
Multi 802.1X
MAC-based Auth.
Selected Counters: The Selected Counters table is visible when the port is in one of the following administrative states:
Multi 802.1X
MAC-based Auth.
The table is identical to and is placed next to the Port Counters table. It is empty if no MAC address is currently selected.
Attached MAC Addresses
Identity: Shows the identity of the supplicant, as received in the Response Identity EAPOL frame. Clicking the link causes the supplicant's EAPOL and Backend Server counters to be shown in the Selected Counters table. If no supplicants are attached, it shows No supplicants attached. This column is not available for MAC-based Auth.
MAC Address: For Multi 802.1X, this column holds the MAC address of the attached supplicant. For MAC-based Auth., this column holds the MAC address of the attached client. Clicking the link causes the client's Backend Server counters to be shown in the Selected Counters table. If no clients are attached, it shows No clients attached.
VLAN ID: This column holds the VLAN ID that the corresponding client is currently secured through the Port Security module
State: The client can either be authenticated or unauthenticated. In the authenticated state, it is allowed to forward frames on the port, and in the unauthenticated state, it is blocked.
If the backend server hasn't successfully authenticated the client, it is unauthenticated. If an authentication fails for one or the other reason, the client remains in the unauthenticated state for Hold Time seconds.
Last Authentication: Shows the date and time of the last authentication of the client (successful and unsuccessful)
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.