17.5.7.1 NAND Flash Boot: NAND Flash Detection
After the NAND Flash interface configuration, a reset command is sent to the memory.
Hardware ECC detection and correction are provided by the PMECC peripheral. See the section PMECC Controller Functional Description for more details.
The Boot Program is able to retrieve NAND Flash parameters and ECC
requirements using two methods as follows:
- The detection of a specific header written at the beginning of the first page of the NAND Flash
- Through the ONFI parameters for the ONFI-compliant memories
Note: Booting on 16-bit NAND Flash is not
possible; only 8-bit NAND Flash memories are supported.