40.8.1 GMAC Network Control Register
Name: | GMAC_NCR |
Offset: | 0x000 |
Reset: | 0x00000000 |
Property: | Read/Write |
Bit | 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | |
IFGQAVCRED | MIIONRGMII | OSSCORR | EXTSELRQEN | PFCCTL | OSSMODE | ||||
Access | R/W | R/W | R/W | R/W | R/W | R/W | |||
Reset | 0 | 0 | 0 | 0 | 0 | 0 |
Bit | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | |
STUDPOFFSET | PTPUNIENA | TXLPIEN | FNP | TXPBPF | ENPBPR | ||||
Access | R/W | R/W | R/W | R/W | R/W | R/W | |||
Reset | 0 | 0 | 0 | 0 | 0 | 0 |
Bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | |
SRTSM | TXZQPF | TXPF | THALT | TSTART | BP | ||||
Access | R/W | R/W | R/W | R/W | R/W | R/W | |||
Reset | 0 | 0 | 0 | 0 | 0 | 0 |
Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
WESTAT | INCSTAT | CLRSTAT | MPE | TXEN | RXEN | LBL | |||
Access | R/W | W | W | R/W | R/W | R/W | R/W | ||
Reset | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bit 30 – IFGQAVCRED Credit-Based Shaping Algorithm Modification
Value | Description |
---|---|
0 | No modification of the CBS algorithm. |
1 | Modifies the CBS algorithm so the IFG/IPG associated with a transmit frame counts towards its 802.1Qav credit. |
Bit 28 – MIIONRGMII MII Control
Value | Description |
---|---|
0 | Disables MII operation. |
1 | Enables MII operation when GMAC_UR.RMII=0. |
Bit 27 – OSSCORR OSS Correction Field
Bit 26 – EXTSELRQEN External Selection of Receive Queue Enable
Value | Description |
---|---|
0 | Disables external selection of receive queue. |
1 | Enables external selection of receive queue. |
Bit 25 – PFCCTL Multiple PFC Pause Quantum Enable
Value | Description |
---|---|
0 | Disables multiple PFC pause quantums. |
1 | Enables multiple PFC pause quantums, one per pause priority. |
Bit 24 – OSSMODE One Step Sync Mode
Value | Description |
---|---|
0 | 1588 One Step Sync mode is disabled. |
1 | 1588 One Step Sync mode is enabled. Replaces timestamp field in the 1588 header for TX Sync Frames with the current TSU timer value. |
Bit 22 – STUDPOFFSET Store UDP Offset
Value | Description |
---|---|
0 | Normal operations. |
1 | The upper 16 bits of the CRC of every received frame are replaced with the offset from start of frame to the beginning of the UDP or TCP header. The lower 16 bits of the CRC are replaced with zero and reserved for future use. The offset is measured in units of 2 bytes. |
Bit 20 – PTPUNIENA Detection of Unicast PTP Frames Enable
Value | Description |
---|---|
0 | Disables detection of unicast PTP frames. |
1 | Enables detection of unicast PTP frames. |
Bit 19 – TXLPIEN Enable LPI Transmission
When set, LPI (low power idle) is immediately transmitted.
Bit 18 – FNP Flush Next Packet
Flush the next packet from the external receive memory. Writing one to this bit will only have an effect if the DMA is not currently writing a packet already stored in the receive memory to system memory.
Value | Description |
---|---|
0 | No effect. |
1 | Flushes the next packet from the receive memory. This will only have an effect if the DMA is not currently writing a packet already stored in the receive memory to system memory. |
Bit 17 – TXPBPF Transmit PFC Priority-based Pause Frame
Value | Description |
---|---|
0 | No effect. |
1 |
Takes the values stored in the Transmit PFC Pause Register. |
Bit 16 – ENPBPR Enable PFC Priority-based Pause Reception
Enables PFC Priority Based Pause Reception capabilities. Setting this bit enables PFC negotiation and recognition of priority-based pause frames.
Bit 15 – SRTSM Store Receive Timestamp to Memory
Value | Description |
---|---|
0 | No effect. |
1 | Causes the CRC of every received frame to be replaced with the value of the nanoseconds field of the 1588 timer that was captured as the receive frame passed the message timestamp point. Note that bit RFCS in register GMAC_NCFGR may not be set to 1 when the timer should be captured. |
Bit 12 – TXZQPF Transmit Zero Quantum Pause Frame
Value | Description |
---|---|
0 | No effect. |
1 | Generates a pause frame with zero quantum to be transmitted. |
Bit 11 – TXPF Transmit Pause Frame
Value | Description |
---|---|
0 | No effect. |
1 | Generates a pause frame to be transmitted. |
Bit 10 – THALT Transmit Halt
Value | Description |
---|---|
0 | No effect. |
1 | Halts transmission as soon as any ongoing frame transmission ends. |
Bit 9 – TSTART Start Transmission
Value | Description |
---|---|
0 | No effect. |
1 | Starts transmission. |
Bit 8 – BP Back pressure
Value | Description |
---|---|
0 | No effect. |
1 | When the MAC is set in 10M or 100M Half Duplex mode, forces collisions on all received frames. |
Bit 7 – WESTAT Write Enable for Statistics Registers
Value | Description |
---|---|
0 | Forces the statistics registers to be in read-only mode for normal operation mode. |
1 | Makes the statistics registers writable for functional test purposes. |
Bit 6 – INCSTAT Increment Statistics Registers
Bit 5 – CLRSTAT Clear Statistics Registers
Value | Description |
---|---|
0 | No effect. |
1 | Clears the statistics registers. |
Bit 4 – MPE Management Port Enable
Value | Description |
---|---|
0 | Forces GMDIO to high impedance state and MDC low. |
1 | Enables the management port. |
Bit 3 – TXEN Transmit Enable
Value | Description |
---|---|
0 | Stops transmission immediately, the transmit pipeline and control registers will be cleared and the Transmit Queue Pointer register will reset to point to the start of the transmit descriptor list. |
1 | Enables the GMAC transmitter to send data. |
Bit 2 – RXEN Receive Enable
When set, RXEN enables the GMAC to receive data. When reset frame reception stops immediately and the receive pipeline will be cleared. The Receive Queue Pointer Register is unaffected.
Value | Description |
---|---|
0 | Stops frame reception immediately and the receive pipeline will be cleared. The Receive Queue Pointer register is unaffected. |
1 | Enables the GMAC to receive data. |
Bit 1 – LBL Loop Back Local
Value | Description |
---|---|
0 | Normal operating mode (no loop back). |
1 | Connects GTX to GRX, GTXEN to GRXDV and forces Full Duplex mode. GRXCK and GTXCK may malfunction as the GMAC is switched into and out of internal loop back. It is important that receive and transmit circuits have already been disabled when making the switch into and out of internal loop back. |