1.1.3.13 SYS_APPDEBUG_Initialize Function
C
int32_t SYS_APPDEBUG_Initialize()Summary
Returns success/ failure for initialization of data structures of the App Debug service
Description
This function is used for initializing the data structures of the App Debug service and is called from within the System Task.
Parameters
index - NULL; reserved for future use init - NULL; reserved for future use
Returns
SYS_APPDEBUG_SUCCESS - Indicates the data structures were initialized successfully
SYS_APPDEBUG_FAILURE - Indicates that it failed to initialize the data structures
Example
if( SYS_APPDEBUG_Initialize(NULL, NULL) == SYS_APPDEBUG_SUCCESS)
{
}Remarks
If the Net system service is enabled using MHC, then auto generated code will take care of system task execution.