1.1.3.12 SYS_APPDEBUG_Deinitialize Function
C
int32_t SYS_APPDEBUG_Deinitialize()Summary
Returns success/ failure for deinitialization of data structures of the App Debug service
Description
This function is used for deinitializing the data structures of the App Debug service and is called from within the System Task.
Parameters
None
Returns
SYS_APPDEBUG_SUCCESS - Indicates the data structures were deinitialized successfully
SYS_APPDEBUG_FAILURE - Indicates that it failed to deinitialize the data structures.
Example
if( SYS_APPDEBUG_Deinitialize() == SYS_APPDEBUG_SUCCESS)
{
}Remarks
If the Net system service is enabled using MHC, then auto generated code will take care of system task execution.