1.7.3.20 SYS_WSS_PingClient Function
C
SYS_WSS_RESULT SYS_WSS_PingClient( uint8_t *data, size_t dataLen, int32_t clientIndex)Summary
Sends a ping message to the client indicated by the parameter clientIndex.
Description
This API sends a ping message to the client indicated by the parameter clientIndex.
Precondition
The connection state of the client indicated by the clientIndex (g_wssSrvcObj.wssState) shall be SYS_WSS_STATE_CONNECTED
Parameters
| Param | Description |
|---|---|
| *data | A pointer to buffer with the data (if any). |
| dataLen | Length of the data |
| clientIndex | The clientID, for identifying the client which caused the event to occur. |
Returns
SYS_WSS_RESULT.
Example
SYS_WSS_RESULT res;
res =SYS_WSS_PingClient(&data, dataLen, 1);Remarks
None.