2.2.31 char * strrchr
char * strrchr(const char *, int) __ATTR_PURE__
The strrchr() function returns a pointer to the last occurrence of the character val in the string src.
Here "character" means "byte" - these functions do not work with wide or multi-byte characters.
Remember:
The strrchr() function returns a pointer to the matched character or NULL if the character is not found.