2.2.33 char * strsep
char * strsep(char **, const char *)
The strsep() function locates, in the string referenced by *sp, the first occurrence of any character in the string delim (or the terminating '\0' character) and replaces it with a '\0'. The location of the next character after the delimiter character (or NULL, if the end of the string was reached) is stored in *sp. An ``empty'' field, i.e. one caused by two adjacent delimiter characters, can be detected by comparing the location referenced by the pointer returned in *sp to '\0'.