2.2.30 char * strpbrk
char * strpbrk(const char *__s, const char *__accept) __ATTR_PURE__
The strpbrk() function locates the first occurrence in the string s of any of the characters in the string accept.
Remember:
The strpbrk() function returns a pointer to the character in s that matches one of the characters in accept, or NULL if no such character is found. The terminating zero is not considered as a part of string: if one or both args are empty, the result will be NULL.