2.1.6 double modf
double modf(double __x, double *__iptr)
The modf() function breaks the argument __x into integral and fractional parts, each of which has the same sign as the argument. It stores the integral part as a double in the object pointed to by __iptr.
The modf() function returns the signed fractional part of __x.
Note:
This implementation skips writing by zero pointer. However, the GCC 4.3 can replace this function with inline code that does not permit to use NULL address for the avoiding of storing.