2.1.36 double fmin
double fmin(double __x, double __y)
The fmin() function returns the lesser of the two values __x and __y. If an argument is NaN, the other argument is returned. If both arguments are NaN, NaN is returned.
double fmin(double __x, double __y)
The fmin() function returns the lesser of the two values __x and __y. If an argument is NaN, the other argument is returned. If both arguments are NaN, NaN is returned.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.