3.8.3.1.2 Code
Add to the main application source file, outside of any functions:
Add to the main application source file, outside of any functions:#define AES_EXAMPLE_REFBUF_SIZE 4uint32_t ref_plain_text[AES_EXAMPLE_REFBUF_SIZE] = {0xe2bec16b,0x969f402e,0x117e3de9,0x2a179373};uint32_t ref_cipher_text_ecb[AES_EXAMPLE_REFBUF_SIZE] = {0xb47bd73a,0x60367a0d,0xf3ca9ea8,0x97ef6624};constuint32_t key128[4] = {0x16157e2b,0xa6d2ae28,0x8815f7ab,0x3c4fcf09};
Copy-paste the following setup code to your user application:/* Output data array */staticuint32_t output_data[AES_EXAMPLE_REFBUF_SIZE];/* State indicate */volatileboolstate =false;structaes_config g_aes_cfg;structaes_module aes_instance;structusart_module usart_instance;
Add to user application initialization (typically the start of main()):staticvoidconfigure_usart(void){structusart_config config_usart;usart_get_config_defaults(&config_usart);config_usart.baudrate = 38400;config_usart.mux_setting = EDBG_CDC_SERCOM_MUX_SETTING;config_usart.pinmux_pad0 = EDBG_CDC_SERCOM_PINMUX_PAD0;config_usart.pinmux_pad1 = EDBG_CDC_SERCOM_PINMUX_PAD1;config_usart.pinmux_pad2 = EDBG_CDC_SERCOM_PINMUX_PAD2;config_usart.pinmux_pad3 = EDBG_CDC_SERCOM_PINMUX_PAD3;stdio_serial_init(&usart_instance, EDBG_CDC_MODULE, &config_usart);usart_enable(&usart_instance);}staticvoidecb_mode_test_dma(void){printf("\r\n-----------------------------------\r\n");printf("- 128bit cryptographic key\r\n");printf("- ECB cipher mode\r\n");printf("- DMA mode\r\n");printf("- 4 32bit words with DMA\r\n");printf("-----------------------------------\r\n");state =false;/* Configure the AES. */g_aes_cfg.encrypt_mode = AES_ENCRYPTION;g_aes_cfg.key_size = AES_KEY_SIZE_128;g_aes_cfg.start_mode = AES_AUTO_START;g_aes_cfg.opmode = AES_ECB_MODE;g_aes_cfg.cfb_size = AES_CFB_SIZE_128;g_aes_cfg.lod =false;aes_set_config(&aes_instance,AES, &g_aes_cfg);/* Set the cryptographic key. */aes_write_key(&aes_instance, key128);/* The initialization vector is not used by the ECB cipher mode. */dma_start_transfer_job(&example_resource_tx);aes_set_new_message(&aes_instance);aes_clear_new_message(&aes_instance);/* Wait DMA transfer */while(false== state) {}/* Wait for the end of the encryption process. */while(!(aes_get_status(&aes_instance) & AES_ENCRYPTION_COMPLETE)) {}state =false;dma_start_transfer_job(&example_resource_rx);/* Wait DMA transfer */while(false== state) {}if((ref_cipher_text_ecb[0] != output_data[0]) ||(ref_cipher_text_ecb[1] != output_data[1]) ||(ref_cipher_text_ecb[2] != output_data[2]) ||(ref_cipher_text_ecb[3] != output_data[3])) {printf("\r\nKO!!!\r\n");}else{printf("\r\nOK!!!\r\n");}}staticvoidtransfer_tx_rx_done(structdma_resource*constresource ){state =true;}staticvoidconfigure_dma_aes_wr(void){structdma_resource_config tx_config;dma_get_config_defaults(&tx_config);tx_config.peripheral_trigger = AES_DMAC_ID_WR;tx_config.trigger_action = DMA_TRIGGER_ACTON_BLOCK;dma_allocate(&example_resource_tx, &tx_config);structdma_descriptor_config tx_descriptor_config;dma_descriptor_get_config_defaults(&tx_descriptor_config);tx_descriptor_config.beat_size = DMA_BEAT_SIZE_WORD;tx_descriptor_config.dst_increment_enable =false;tx_descriptor_config.block_transfer_count = AES_EXAMPLE_REFBUF_SIZE;tx_descriptor_config.source_address = (uint32_t)ref_plain_text +sizeof(ref_plain_text);tx_descriptor_config.destination_address =(uint32_t) &(AES->INDATA);dma_descriptor_create(&example_descriptor_tx, &tx_descriptor_config);dma_add_descriptor(&example_resource_tx, &example_descriptor_tx);}staticvoidconfigure_dma_aes_rd(void){structdma_resource_config rx_config;dma_get_config_defaults(&rx_config);rx_config.peripheral_trigger = AES_DMAC_ID_RD;rx_config.trigger_action = DMA_TRIGGER_ACTON_BLOCK;dma_allocate(&example_resource_rx, &rx_config);structdma_descriptor_config rx_descriptor_config;dma_descriptor_get_config_defaults(&rx_descriptor_config);rx_descriptor_config.beat_size = DMA_BEAT_SIZE_WORD;rx_descriptor_config.src_increment_enable =false;rx_descriptor_config.block_transfer_count = AES_EXAMPLE_REFBUF_SIZE;rx_descriptor_config.source_address = (uint32_t)&(AES->INDATA);rx_descriptor_config.destination_address =(uint32_t)output_data +sizeof(output_data);dma_descriptor_create(&example_descriptor_rx, &rx_descriptor_config);dma_add_descriptor(&example_resource_rx, &example_descriptor_rx);}
/* Initialize the system and console*/system_init();configure_usart();/* Configure AES DMA and enable callback */configure_dma_aes_wr();configure_dma_aes_rd();dma_register_callback(&example_resource_tx, transfer_tx_rx_done,DMA_CALLBACK_TRANSFER_DONE);dma_enable_callback(&example_resource_tx, DMA_CALLBACK_TRANSFER_DONE);dma_register_callback(&example_resource_rx, transfer_tx_rx_done,DMA_CALLBACK_TRANSFER_DONE);dma_enable_callback(&example_resource_rx, DMA_CALLBACK_TRANSFER_DONE);aes_get_config_defaults(&g_aes_cfg);aes_init(&aes_instance,AES, &g_aes_cfg);aes_enable(&aes_instance);