13.8.1.1.3 Workflow
- Create a PORT module pin configuration struct, which can be filled out to adjust the configuration of a single port pin.
structport_config config_port_pin; - Initialize the pin configuration struct with the module's default values.
port_get_config_defaults(&config_port_pin);Note: This should always be performed before using the configuration struct to ensure that all values are initialized to known default settings. - Adjust the configuration struct to request an input pin.
config_port_pin.direction = PORT_PIN_DIR_INPUT;config_port_pin.input_pull = PORT_PIN_PULL_UP; - Configure push button pin with the initialized pin configuration struct, to enable the input sampler on the pin.
port_pin_set_config(BUTTON_0_PIN, &config_port_pin); - Adjust the configuration struct to request an output pin.
config_port_pin.direction = PORT_PIN_DIR_OUTPUT;Note: The existing configuration struct may be re-used, as long as any values that have been altered from the default settings are taken into account by the user application. - Configure LED pin with the initialized pin configuration struct, to enable the output driver on the pin.
port_pin_set_config(LED_0_PIN, &config_port_pin);