3 Run PROGRAM Action for Splash Kit
(Ask a Question)After generating the bitstream, the PolarFire device must be programmed. To program the PolarFire device, perform the following steps:
- Ensure that the jumper settings on the board are the same as those listed in the following table.
Table 3-1. Jumper Settings Jumper Description J5, J6, J7, J8, and J9 Short pin 2 and 3 for programming the PolarFire® FPGA through FTDI J11 Short pin 1 and 2 for programming through the FTDI chip J10 Short pin 1 and 2 for programming through the FTDI SPI J4 Short pin 1 and 2 for manual power switching using SW1 J3 Open pin 1 and 2 for 1.0V - Connect the power supply cable to the J2 connector on the board.
- Connect the USB cable from the Host PC to J1 (FTDI port) on the board.
- Power on the board using the SW1 slide switch.
Figure 3-1. Splash Kit Board Setup 
- Double click Run PROGRAM Action from the Libero > Design Flow tab.
When the device is programmed successfully, a green tick mark appears, as shown in the following figure. See Running the Demo to run the PCIe EndPoint demo.