8 Appendix 4: Programming the Device Using FlashPro Express
(Ask a Question)This section describes how to program the PolarFire device with the
.job programming file using FlashPro Express. The
.job file is available at the following design
files folder location:
mpf_an4597_df\Programming_files
To program the device, perform the following steps:
- Ensure that the jumper settings on the board are the same as listed in Table 2-1 (for evaluation) and Table 3-1 (for splash).Important: The power supply switch must be switched off while making the jumper connections.
- Connect the power supply cable to the J9 connector on the Evaluation board or J2 connector on the Splash board.
- Connect the USB cable from the Host PC to the J5 (FTDI port) on the Evaluation board or J1 (FTDI port) on the Splash board.
- Power on the board using the SW3 slide switch on the Evaluation board or SW1 slide switch on the Evaluation board.
- On the host PC, launch the FlashPro Express software.
- To create a new job, click New or in the Project menu, select New Job Project from FlashPro Express Job.
- Enter the following in the New Job Project from FlashPro Express Job dialog box:
- Programming job file: Click Browse, navigate to the location where the .job file is located, and select the file. The default location is: <download_folder>\mpf_an4597_df\Programming_files.
- FlashPro Express job project location: Click Browse and navigate to the location where you want to save the project.
Figure 8-1. New Job Project from FlashPro Express Job 
- Click OK. The required programming file is selected and ready to be programmed in the device.
- The FlashPro Express window appears, as shown in the following figure. Confirm that a programmer number appears in the Programmer field. If it does not, confirm the board connections and click Refresh/Rescan Programmers.
Figure 8-2. Programming the Device - Click RUN. When the device
is programmed successfully, a RUN PASSED
status is displayed as shown in the following figure. To run the
PCIe EndPoint demo, see Running the Demo
section.
Figure 8-3. FlashPro Express—RUN PASSED - Close FlashPro Express or in the Project tab, click Exit.