2 Run PROGRAM Action for Evaluation Kit
(Ask a Question)After generating the bitstream, the PolarFire device must be programmed. To program the PolarFire device, perform the following steps:
- Ensure that the jumper settings on the board are the same as those listed in the following table.
Table 2-1. Jumper Settings Jumper Description J18, J19, J20, J21, and J22 Short pin 2 and 3 for programming the PolarFire® FPGA through FTDI J28 Short pin 1 and 2 for programming through the on-board FlashPro5 J26 Short pin 1 and 2 for programming through the FTDI SPI J27 Short pin 1 and 2 for programming through the FTDI SPI J4 Short pin 1 and 2 for manual power switching using SW3 J12 Short pin 3 and 4 for 2.5V - Connect the power supply cable to the J9 connector on the board.
- Connect the USB cable from the Host PC to J5 (FTDI port) on the board.
- Power on the board using the SW3 slide switch.
Figure 2-1. Evaluation Kit Board Setup - Double click Run PROGRAM Action from the Libero > Design Flow tab.