11 Revision History

The revision history describes the changes that were implemented in the document. The changes are listed by revision, starting with the current publication.

Table 11-1. Revision History
RevisionDateDescription
D09/2025The following is the list of changes in revision D of the document:
C02/2025The following is the list of changes in revision C of the document:
B02/2024The following is the list of changes in revision B of the document:
A08/2022The following is the list of changes in revision A of the document:
10.0—Added Appendix 5: Running the TCL Script.
9.0—The following is a summary of the changes made in this revision.
  • Updated the document for Libero SoC v12.3.
  • Removed the references to Libero version numbers.
8.0—The document was updated for Libero SoC v12.0 release.
7.0—Merged Splash kit related content and updated the document for Libero SoC PolarFire v2.3 release.
6.0—The following is a summary of the changes made in revision 6.0 of this document.
5.0—The document was updated for Libero SoC PolarFire v2.1 release.
4.0—The document was updated to include features and enhancements introduced in the Libero SoC PolarFire v2.0 release.
3.0—The following is a summary of the changes made in revision 3.0 of this document.
2.0—The following is a summary of the changes in revision 2.0 of this document.
  • The document was updated for Libero SoC PolarFire v1.1 release.
  • Information about resource utilization was added. For more information, see Resource Utilization.
1.0—The first publication of this document.